On November 12, the 15th China International Aviation and Aerospace Exhibition was grandly opened in Zhuhai.The attention of the global aerospace field gathered here. At this grand event where technology and innovation meet, T-motor, as a pioneer brand of UAV/drone propulsion systems, brought a series of innovative products to the show.

1、S series manned power
Specially designed for E-VTOL aircraft, it adopts an innovative structure, with efficient air cooling and heat dissipation and ultra-durable operation capabilities. It supports 400V high-voltage drive, which is stable and reliable. At present, the series includes 3 models, and the maximum thrust range of a single motor is 100~200kg.



2、A series modular propulsion system
A new platform modular propulsion system, specially developed for multi-rotor UAVs. It is suitable for multiple application scenarios such as agricultural plant protection, logistics, education and training, aerial filming and photography, etc.


3、VL series propulsion system
Designed for the rotor power needs of VTOL UAVs, it has electronic adaptive locking propeller technology, which is energy-efficient and reliable. At the same time, it is equipped with a temperature sensor with direct connection to the flight control system to ensure of safety.


During this magnificent air show trip, T-MOTOR would like to express our sincere gratitude to everyone who visited our booth and partners who gave us support. In the future, T-MOTOR will continue to forge ahead, giving back to users with better products and services, and work together with you to create a better future for the development of the industry.